SUSO Sondermaschinenbau GmbH

Blanking plant for printing plates with S7-1500/ S7-1200/ET 200AL

„In order to meet the automotive branche‘s high requirements, it is important to us to cooperate with reliable suppliers ourselves.”

Customer

Place

Industries

Used Products

Customer profile & project information

Suso Sondermaschinenbau GmbH is a german engineering company located in Sulzbach-Rosenberg.  Founded in 1994, the company is mainly building special machinery for the processing of metals, ceramics and polymers via 3D-milling, drilling, sanding or blanking.

Challenges

  • Reducing downtimes
  • Cutting down probability of error during programming and easier handling of changes
  • Accurate display output with a great deal of information at once

Solution

Mounted on a tool holder system, the printing plates are automatically being processed running through a total of 13 process stations. The plant’s capacity can be maxed out, thus allowing for an unattended run over a certain period of time. This way operation can be maintained in between working shifts.

Customer benefit

  • 45% time saving at spare part changes. Labelling enables good traceability.
  • Programming mistakes can be avoided with the help of an array indicated SCL-coding, which can be used on any controller.
  • The comfort panels‘  high resolution and accurate handling allow  for a quick access to requested information via touch command.