AC Schwimmbadtechnik AG

Refreshingly easy with crystal-clear benefits

"In our company where, in effect, a single person carries out all the engineering, we appreciate the excellent support provided by the TIA Portal – specifically the generation of links for the exchange of parameters between HMI and CPU is really very helpful"Markus Achermann, CEO

Customer

Place

Industries

Used Products

Customer profile and project information

As one of the leading swimming pool construction companies in the Alps region, AC Schwimmbadtechnik serves several target groups – from private customers to commercial users. To be able to win over the various customers with their requirements, the company needs flexible systems and a sustainable concept. In SIEMENS, they have found a partner who can provide them with all of that. 

Challenges

To satisfy the customers' requirements, AC Schwimmbadtechnik must simplify its engineering phase. One person should be able to intuitively configure all of the components. In addition, the company needs a flexible system with easy operation of the pool systems so that customers themselves can control the system.

Solution

To best serve the customer, AC relies on the TIA Portal. In addition to the integration of the controller, drives and HMI in one system, the individual hardware components such as a Basic Panel 2nd Gen., the S7-1200 controller and the SINAMICS V20 bring real added value.

Customer benefits

  • Time/cost savings… through simple exchange of parameters between PLC and HMI
  • Reduced workload for additional customer requirements… due to device replacement at the click of a mouse
  • Effective customer training… by using visualization instead of status LEDs